Skip to main content
Jameszhan
Associate
July 1, 2020
Question

how to create the PFC feature code with STEVAL-CTM010V1 board

i got a STEVAL-CTM010V1 board and installed the SDK(5.4.4 full),after that i created a project base on example(STEVAL-CTM010V1 dual drive with PFC,see pic_1),but the example does not enable the PFC feature(see pic_2),so if we want to use the PFC feature on CTM010V1 board ,what should we do ?

This topic has been closed for replies.

5 replies

Jameszhan
JameszhanAuthor
Associate
July 1, 2020

@Claire OKU (ST Employee)​ 

Jameszhan
JameszhanAuthor
Associate
July 2, 2020

i found a tips to fix this issue,just need to modify the config.xml file(C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.4.4\Utilities\PC_Software\STMCWB\assets\xml).

hence,if you remove the warning ,you can config the PFC feature on WB.

.

RRach.2
Visitor II
August 30, 2022

Hi Jameszhan,

Is it safe doing that?

Best Regards,

Rado

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Lmazz.1
Visitor II
November 16, 2023

Any solution to this ?

many thanks