Skip to main content
1123
Associate II
Apr 28, 2025 7:02 AM UTC
Solved

How to create graphics using Motor Pilot

Hi all ,

I’m currently using the EVSPIN32G development board to run six-step trapezoidal commutation.
I’m using Motor Pilot version V1.2.12 with the MC_6STEP GUI.

In the ST Motor Control tutorial under '6-step - Optimization and troubleshooting of sensor-less firmware parameters,' I saw several phase voltage (BEMF U/V/W) waveforms. However, in Motor Pilot I can only find 'bus voltage' and 'bemf_ADC_conf'—I don’t see any options related to viewing BEMF U/V/W voltages directly. Could you please advise how I can access these waveforms, or if there’s an additional setting or tool needed to display them?

未命名.png

未命名2.png

Thanks.

This topic has been closed for replies.
Fabrice LOUBEYRE
Fabrice LOUBEYREBest answer
ST Employee
Apr 28, 2025 10:11 AM UTC

Hi 1123,

unfortunately, you will have not access to any BEMF signals with the Motor Pilot of the MCSDK6.3.2 or next versions. This is due to the fact that the Zero crossing detection of the BEMF is managed with the Watchdog feature of the corresponding ADC and in consequence no access to the data directly by the FW.

The  BEMF_ADC_CONF register contains only BEMF Sensing parameters of the algorithm.

Best regards.

Fabrice

 

 

 

1 reply

Fabrice LOUBEYRE
Fabrice LOUBEYREBest answer
ST Employee
Apr 28, 2025 10:11 AM UTC

Hi 1123,

unfortunately, you will have not access to any BEMF signals with the Motor Pilot of the MCSDK6.3.2 or next versions. This is due to the fact that the Zero crossing detection of the BEMF is managed with the Watchdog feature of the corresponding ADC and in consequence no access to the data directly by the FW.

The  BEMF_ADC_CONF register contains only BEMF Sensing parameters of the algorithm.

Best regards.

Fabrice