Skip to main content
Associate
Jun 8, 2025 2:56 PM UTC
Question

How to cool B-D431B-ESC1

I saw in a post here that someone blew up their B-G431B-ESC1 with just 5As using the motor profiler. The spec says the mosfets will output up to 120A. I am looking to run motors up to 30A. I'd like to see if there is a prescribed way of adding heat sink & fan to controller board.

 

This topic has been closed for replies.

3 replies

Senior III
Jun 8, 2025 3:47 PM UTC

Even 5 A may be too much for a passive board in some situations without additional cooling or a current limit set properly.

robomowAuthor
Associate
Jun 8, 2025 4:38 PM UTC

Duh, Obviously.

Thats why I am asking if there ar existing heat sinks and mounting proceedures. My other motor controllers like flipsky FESc nd ODrive have substaintial heat sinks on them.

Witho¨t mountingholes and very small footprint. Seems like a big issue to cool this bord for higher current motors.'

GMA
ST Technical Moderator
Jul 10, 2025 2:10 PM UTC

Hello @robomow,

It is mentioned in data brief document: "Output peak motor current (maximum peak current tested with propeller to have an air-forced cooling:( 40 A"

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA