Skip to main content
TNITT.2
Associate
Sep 2, 2020 4:35 AM UTC
Question

How to configure ioc file to operate STEVAL-SPIN3202 board with MC Workbench?

Original title is (before moderator's edit):

"I tried to operate STEVAl-SPIN3202 board.

But I couldn't operate.

I'd like to solve the issue one by one. 

So, please support me or send the advice."

I want to operate STEVAL-SPIN3202 board by library on CubeIDE 1.4.2 with CubeMX 6.0. I.

First I made ioc fail to used Mortor Control Work Bench 5.4.4.

So, I download and load STEVAL-SPIN3202_HALL_SDK544.stmx file.

In the created ioc file, STM32 model number is STM32F031C6Tx.

But actual model number in STEVAl-SPIN 3202 board is STM32F103C8Tx.

Is it necessary to make ioc file by manual?

is It ok to used STEVAL-SPIN3202_HALL_SDK544.stmx file?

Please teach me or send the advice.

My enviromente is following.

        PC : Windows 10

        STM32Cube MX : Version 6.0.1

        STMCube IDE : version 1.4.2

       Motor Control Workbench : 5.4.4

This topic has been closed for replies.

7 replies

Khouloud OTHMAN
Associate
Sep 2, 2020 3:57 PM UTC

Hello TNITT.2,

As I understand you have used Motor Control Workbench to create .stmcx project then you run the generated CubeMx project.

I doubt that this an STM32CubeMX problem, it is more related to ST Motor Control, so it will be more helpful to post this question under https://community.st.com/s/topic/0TO0X000000BSrWWAW/motor-control-firmware-and-software.

Regards,

Khouloud.

TNITT.2
TNITT.2Author
Associate
Sep 3, 2020 6:21 AM UTC

​Dear Khouloud,

Hello.

Thank you for your reply and advice.

I ask my question at your indicated place.

Laurent Ca...
Senior III
Sep 18, 2020 1:10 PM UTC

Dear TNITT.2

Could you give a real title (as short as possible) at your post in order to make the forum useful for everyone and not copy a chat sentence.

Thanks by advance.

Laurent C.

Laurent Ca...
Senior III
Sep 22, 2020 7:47 AM UTC

Dear TNITT.2

I changed the tilte of this post from :

    "I tried to operate STEVAl-SPIN3202 board.

    But I couldn't operate.

    I'd like to solve the issue one by one.

    So, please support me or send the advice." (that I moved in your text message)

to:

    "How to configure ioc file to operate STEVAL-SPIN3202 board with MC Workbench?"

Please do not hesitate to change it again if you need.

Thanks for your understanding.

Laurent C.

PBo
Visitor II
Oct 22, 2020 7:36 AM UTC

​@TNITT.2​ 

Hello,

Please, could indicate if you are using 6-steps or FoC algorithm ?

However, and FYI, the STEVAL-SPIN3202 board is embedding a STM32F031 MCU.

Thanks a lot,

Best Regards,

PBo

Cristiana SCARAMEL
ST Employee
Oct 22, 2020 9:14 AM UTC

Hello @TNITT.2​ 

where did STEVAL-SPIN3202_HALL_SDK544.stmx come from?

Moreover, the STEVAL-SPIN3202 is an evaluation board based on the STSPIN32F0A (system in package with STM32F031C6 MCU integrated).

Please, share with us more details on your application requirements as abovementioned by @PBo​ for a better support.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Laurent Ca...
Senior III
Nov 2, 2020 8:51 AM UTC

Dear @TNITT.2​ 

As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...