How to ACTUALLY get started with STEVAL-SPIN3202 ??
In order to actuate a gripper prototype, I decided to buy a BLDC motor from Maxon (EC-32 flat), and an evaluation board to drive it (STEVAL-SPIN3204, then STEVAL-SPIN3202).
After setting up the hardware connection with the STEVAL-SPIN3204, I manage to launch the example that was presented in MC workbench. The result was a motor not spinning, vibrating, and the program stopping after a few seconds. After a lot of time wasted in trying to get things working by twicking in the monitoring window, I decided to buy another board (STEVAL-SPIN3202) that was actually compatible with MC Workbench.
Setting up the hardware again, and figuring out the jumpers thingys based on the obscure documentation of the board, and being able to finally create my own project on MCW, I try to hopfully launch the compiled bin on the board, but nothing. On top of that, impossible to even connect the board through UART to the monitoring window.
So now, I am kindly asking for guidance on how to actually set up PROPERLY one of those board, and what could be the detailed steps to follow to be able to control the motor using a Hall sensor, a position sensor and the torque feedback of the board.
Thank you in advance for your answers,
Best
Arthur CANDALOT