Skip to main content
HSing.5
Associate
Jan 14, 2025 8:43 AM UTC
Question

How run motor using PWM in STSPIN32F0A

I have a STSPIN32F0A board on which, I need support on below points

1) Ability to operate the motor through LIN/PWM signal rather than an ADC signal, currently the EVAL board supports an ADC through an onboard potentiometer which I want to remove. 

2) My current design is not able to move beyond 1.5A rms, whereas the design can support up to 15A rms, How to rectify this issue?

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Jul 17, 2025 2:10 PM UTC

Hello @HSing.5,

Firstly, we would like to apologize for the delay in replying to your post.
If your point is still pertinent, you can generate as example, a project with STEVAL-SPIN3202 board (that embeds a STSPIN32F0A MCU) available on MCSDK-6.4.0.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA