Skip to main content
MAnde.11
Associate II
April 25, 2023
Solved

How do I operate motor profiler from Motor Pilot V1.1.5?

Whenever I detect boards, the software tells me it needs to update the firmware on the target. Then it pops up a dialog that says it is checking ST-Link connection. However, it says in this state forever without error or progress. How can I either install the fw it wants ahead of time or convince it that the connection is fine?

This topic has been closed for replies.

10 replies

ST Employee
April 26, 2023

Hello @MAnde.11​ , we are currently working on a profiler fix, can you replace the attached file "profiler.qml" in your "Motor Pilote" folder at location "MC_SDK_6. 1.1\Utilities\PC_Software\STMotorPilot\GUI" and remove all binaries that are not 6.1.1 at the location "MC_SDK_6.1.1\Utilities\PC_Software\STMotorPilot\STM32CubeProgrammer\Fw"

Normally you should have no more problems. Can you confirm that it works please? 

thank you

"If you agree with my answer, please accept it by clicking on ""Accept as solution""."
MAnde.11
MAnde.11Author
Associate II
April 26, 2023

Unfortunately it still has the same issue (hangs at the Check St-Link connection part).

I unzipped the attached file, and replace the profiler.qml file in the GUI directory. I also deleted all 6.1.0 and 6.0.0 files from the Fw directory.

SamHansen42
SamHansen42Best answer
Associate II
May 1, 2023
MAnde.11
MAnde.11Author
Associate II
May 2, 2023

Wow, thanks for taking time to post this even after you found a solution. To be clear, I just installed it in C:/ST/something and it worked out of the box. Probably something about space in the path.