Skip to main content
Dror Laor
Visitor II
March 20, 2017
Question

How can I use Motor Profiler with STEVAL-SPIN3201?

Posted on March 20, 2017 at 15:10

I noticed that STEVAL-SPIN3201 is not on the supported boards list for Motor Profiler. Is there an update/path?

This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
March 22, 2017
Posted on March 22, 2017 at 10:28

Unfortunately the Motor Profiler does not support the STM32 embedded into the STSPIN32F0 System-in-package.

In any case, you can use the Motor Profiler using one of the supported boards and then 'export' the results on the STEVAL-SPIN3201 using the MC Workbench 

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards