Skip to main content
Jace
Associate II
April 19, 2020
Question

How can I convert additional regular conversion?

I'm using MCSDK_v5.4.3 but I don't know how can I convert additional ADC channel.

Below is ADC initialization code. added channel 9 and 10.

But I can't convert channel 9 and 10.

How can I convert ch.9 & 10.

Some sample code will very helpful to me.

Thanks

​

​

static void MX_ADC1_Init(void)

{

​

 /* USER CODE BEGIN ADC1_Init 0 */

​

 /* USER CODE END ADC1_Init 0 */

​

 ADC_InjectionConfTypeDef sConfigInjected = {0};

 ADC_ChannelConfTypeDef sConfig = {0};

​

 /* USER CODE BEGIN ADC1_Init 1 */

​

 /* USER CODE END ADC1_Init 1 */

 /** Common config 

 */

 hadc1.Instance = ADC1;

 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV1;

 hadc1.Init.Resolution = ADC_RESOLUTION_12B;

 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;

 hadc1.Init.ContinuousConvMode = DISABLE;

 hadc1.Init.DiscontinuousConvMode = DISABLE;

 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;

 hadc1.Init.DataAlign = ADC_DATAALIGN_LEFT;

 hadc1.Init.NbrOfConversion = 4;

 hadc1.Init.DMAContinuousRequests = DISABLE;

 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

 hadc1.Init.LowPowerAutoWait = DISABLE;

 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;

 if (HAL_ADC_Init(&hadc1) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Injected Channel 

 */

 sConfigInjected.InjectedChannel = ADC_CHANNEL_1;

 sConfigInjected.InjectedRank = ADC_INJECTED_RANK_1;

 sConfigInjected.InjectedSingleDiff = ADC_SINGLE_ENDED;

 sConfigInjected.InjectedNbrOfConversion = 3;

 sConfigInjected.InjectedSamplingTime = ADC_SAMPLETIME_19CYCLES_5;

 sConfigInjected.ExternalTrigInjecConvEdge = ADC_EXTERNALTRIGINJECCONV_EDGE_RISING;

 sConfigInjected.ExternalTrigInjecConv = ADC_EXTERNALTRIGINJECCONV_T1_TRGO;

 sConfigInjected.AutoInjectedConv = DISABLE;

 sConfigInjected.InjectedDiscontinuousConvMode = DISABLE;

 sConfigInjected.QueueInjectedContext = ENABLE;

 sConfigInjected.InjectedOffset = 0;

 sConfigInjected.InjectedOffsetNumber = ADC_OFFSET_NONE;

 if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)

 {

Error_Handler();

 }

 /** Configure Injected Channel 

 */

 sConfigInjected.InjectedChannel = ADC_CHANNEL_7;

 sConfigInjected.InjectedRank = ADC_INJECTED_RANK_2;

 if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Injected Channel 

 */

 sConfigInjected.InjectedChannel = ADC_CHANNEL_6;

 sConfigInjected.InjectedRank = ADC_INJECTED_RANK_3;

 if (HAL_ADCEx_InjectedConfigChannel(&hadc1, &sConfigInjected) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_2;

 sConfig.Rank = ADC_REGULAR_RANK_1;

 sConfig.SingleDiff = ADC_SINGLE_ENDED;

 sConfig.SamplingTime = ADC_SAMPLETIME_61CYCLES_5;

 sConfig.OffsetNumber = ADC_OFFSET_NONE;

 sConfig.Offset = 0;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_8;

 sConfig.Rank = ADC_REGULAR_RANK_2;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN ADC1_Init 2 */

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_9;

 sConfig.Rank = ADC_REGULAR_RANK_3;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

​

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_10;

 sConfig.Rank = ADC_REGULAR_RANK_4;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE END ADC1_Init 2 */

​

}

​

This topic has been closed for replies.

5 replies

TDK
April 19, 2020

Are you saying this code converts channels 2 and 8 just fine but doesn't convert 9 and 10? Seems odd.

Make sure you're initializing the pins for channels 9/10.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Jace
JaceAuthor
Associate II
April 19, 2020

I added initializing code for 9 & 10 and pin assignment also as below.

void HAL_ADC_MspInit(ADC_HandleTypeDef* hadc)

{

 GPIO_InitTypeDef GPIO_InitStruct = {0};

 if(hadc->Instance==ADC1)

 {

  __HAL_RCC_ADC1_CLK_ENABLE();

  __HAL_RCC_GPIOC_CLK_ENABLE();

  __HAL_RCC_GPIOA_CLK_ENABLE();

  GPIO_InitStruct.Pin = M1_CURR_AMPL_W_Pin|M1_CURR_AMPL_V_Pin|M1_TEMPERATURE_Pin|ADC_9_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);

  GPIO_InitStruct.Pin = M1_CURR_AMPL_U_Pin|M1_BUS_VOLTAGE_Pin|ADC_10_Pin;

  GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 }

}

What I want to ask is how can I use below functions related regular conversion.

such as

uint8_t RCM_RegisterRegConv(RegConv_t * regConv);

uint8_t RCM_RegisterRegConv_WithCB (RegConv_t * regConv, RCM_exec_cb_t fctCB, void *data);

uint16_t RCM_ExecRegularConv (uint8_t handle);

bool RCM_RequestUserConv(uint8_t handle);

uint16_t RCM_GetUserConv(void);

void RCM_ExecUserConv (void);

RCM_UserConvState_t RCM_GetUserConvState(void);

Thanks

MR.3
Associate
June 23, 2020

Hello,

Did you resolve the above issue??

if yes can you please let me know the solution?

Thank you.

Laurent Ca...
Senior III
October 14, 2020

Dear @Jace​ 

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
October 26, 2020

Dear @Jace​ 

I guess you don't have to solve this problem anymore, therefore I consider this thread closed.

If not, feel free to reopen it by posting an answer.

Best regards

Laurent Ca...