Skip to main content
MRyan.7
Associate III
January 16, 2019
Solved

How are signals PHASE_1, 2, and 3 used in the ST-EVAL-ESC01 design?

In trying to create a design from scratch using the motor control workbench, I have tried to verify what I see in the ST-EVAL-ESC01 design documentation. In that design (https://www.st.com/en/embedded-software/stsw-esc001v1.html) that there are three phase_x signals, three curr_fdbk x signals, and three vshunt_x_filtered signals. See here:

0690X000006D77aQAC.png

In a startup program using the STM32F303 and Workbench 5.1, it is pretty clear that the current feedback is accounted for (A0/A1/A2) and the over current protection (A7/B9/B11) is for the vshunt_x_filtered signals. Here:

0690X000006D77fQAC.png

I see nothing in the workbench that accommodates the PHASE_x signals.

What are they used for (if at all) in this design?

Thanks,

Mr. Yan

This topic has been closed for replies.
MRyan.7
MRyan.7Best answer
Associate III
January 21, 2019

For others....

This was resolved by Cedric in a separate thread. The PHASE_X signals are not used in this design (i.e. for FOC control).

2 replies

MRyan.7
MRyan.7AuthorBest answer
Associate III
January 21, 2019

For others....

This was resolved by Cedric in a separate thread. The PHASE_X signals are not used in this design (i.e. for FOC control).

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards