Skip to main content
Low Yik Seong
Associate III
Apr 29, 2018 2:41 PM UTC
Question

high side and low side pwm idle state

Posted on April 29, 2018 at 16:41

Hi, I would like to ask what is the function of pwm idle state which can be selected in drive management in sdk 5.0? It only can be turn off as I tried turn them on they would be fatal error as I compile the code.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
Jun 15, 2021 6:57 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards