Skip to main content
Visitor II
June 27, 2023
Question

High Dynamic Low Ripple Setup

Dear forum,

For my research project I need to generate arbitrary torque spectrums. Ideally with frequencies of up to 3.5kHz. I planned on using a ~200W PMSM and am now wondering which STM microcontroller and motor control board would be best suited for this task. Note that I don't plan on heavily modifying the control structures of the Motor Control SDK. This would likely take too much time. Is this even possible with the STM motor control ecosystem? If not, do you have any suggestions for me?

Thank you very much!
Max

    This topic has been closed for replies.

    1 reply

    ST Employee
    July 7, 2023

    Hello, could you please describe the use case more precisely? Otherwise, based on the information provided, it seems that a G4 or F4 could work. I am waiting for your response to refine my answer. Thank you.

    "If you agree with my answer, please accept it by clicking on ""Accept as solution""."