Skip to main content
Ryada.1
Associate III
Aug 13, 2020 6:25 AM UTC
Solved

Hi sir this is rahul yadav working in greenfield control system r & d , sir i am using steval 3202 board sir i want to spin bldc motor with hall sensor i am usinf stspin motor control work bench but motor is doing noise and torque is not up to the ma

what parameter should i enter for hall sensored foc control in motor control work bench any pdf available for hall sensored foc control in motor control work bench 5.2.0 sir problem is motor is spining but torque is less any guidlines availble to run motor using hall sensor foc on stm site

This topic has been closed for replies.
Cristiana SCARAMEL
ST Employee
Sep 17, 2020 9:33 AM UTC

Hi @Ryada.1​ ,

firstly did you change the board setting to use the Hall sensors feedback?

Please refer to user manual UM2278 for a detailed description (section 2.2.2 at page 9).

Moreover could you give us more details on your application?

- Driving method: six-step or Field Oriented Control algortihm?

- Power supply voltage?

- Motor parameters or part number?

Concerning the firmware package and STM32 motor control workbench you can find dedicate user manuals UM2310 and UM2168 in the Resource tab of STEVAL-SPIN3202 board page

Let me know if your motor finally runs ;)

"If you feel a post has answered your question, please click ""Accept as Solution"""

9 replies

TNITT.2
Associate
Sep 2, 2020 8:18 AM UTC

​Dear Ryada.1

I also try to operate steval 3202 board with motor control work bench.

I have question.

How did you make stmx file?

Did you use STEVAL-SPIN3202_HALL_SDK544.stmx file?

Please inform me.

Ryada.1
Ryada.1Author
Associate III
Sep 6, 2020 12:36 PM UTC

No I use motor control workbench 5.4.2​

Ryada.1
Ryada.1Author
Associate III
Sep 6, 2020 12:38 PM UTC

And it generates. stmx ​file after doing all the steps you need to follow motor control workbench operating process

TNITT.2
Associate
Sep 7, 2020 7:14 AM UTC

Dear Ryada.1

Thank you for your information.

TNITT.2
Associate
Sep 8, 2020 4:06 AM UTC

​Dear Ryada.1

I have not  operate steval 3202 board yet .

Could you send ioc file or your operating environment to me, please?

Cristiana SCARAMEL
ST Employee
Sep 17, 2020 9:33 AM UTC

Hi @Ryada.1​ ,

firstly did you change the board setting to use the Hall sensors feedback?

Please refer to user manual UM2278 for a detailed description (section 2.2.2 at page 9).

Moreover could you give us more details on your application?

- Driving method: six-step or Field Oriented Control algortihm?

- Power supply voltage?

- Motor parameters or part number?

Concerning the firmware package and STM32 motor control workbench you can find dedicate user manuals UM2310 and UM2168 in the Resource tab of STEVAL-SPIN3202 board page

Let me know if your motor finally runs ;)

"If you feel a post has answered your question, please click ""Accept as Solution"""
Ryada.1
Ryada.1Author
Associate III
Oct 12, 2020 8:40 AM UTC

thanks for reply i have changed jumper setting now a am using encoder for speed sensing , and i have read the manual but there is no explanation about how to set speed and torque pid in any manual my motor is 2400 rpm 4 pole bldc motor

Ryada.1
Ryada.1Author
Associate III
Oct 12, 2020 8:43 AM UTC

i am using st motor workbench foc algorithm speed sensing with encoder

Laurent Ca...
Senior III
Oct 13, 2020 7:14 AM UTC

Dear @Ryada.1​ 

If you have a new question, please open a new thread.

Best regards

Laurent Ca...