Skip to main content
JCHEN.4
Associate II
December 14, 2018
Question

Hi, I need to apply HFI for controlling a sensorless BLDC motor in low speed. However, the speed sensor option of 'HFI+Observer' in the STM32 SDK 5.3.1 workbench is not supported. How to address this problem? Thanks!

..

This topic has been closed for replies.

3 replies

JCHEN.4
JCHEN.4Author
Associate II
December 18, 2018

It seems that the feature is available in older version of SDK such as 4.3. However, I could not find any old version installation package online now. Any idea?

cedric H
ST Technical Moderator
January 2, 2019

The HFI feature is not supported for the moment because we are not able to find a motor matching HFI requirement in order to test it.

If you do have such kind of motor that is able to do HFI with 4.3 release please let us know.

Regards

Cedric

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards