Skip to main content
MCseh.377
Associate
October 12, 2019
Question

Hi, I just ordered an X-NUCLEO-IHM02A1 and I have a NUCLEO-F411RE - STM32 Nucleo-64 development board. Can I use those two together? If not, which Nucleo board have to buy to use the stepper driver ODE?

  • October 12, 2019
  • 1 reply
  • 1035 views

This is for a project. I develop a drwaing machine, 2 axis -> 2 steppers for x-y coordinates.

This topic has been closed for replies.

1 reply

Cristiana SCARAMEL
ST Employee
October 26, 2023

The X-NUCLEO-IHM02A1 expansion board is designed to permit the use of any STM32 Nucleo board.

The X-CUBE-SPN2 expansion software package is compatible with the NUCLEO-F401RE, the NUCLEO-F302R8
or the NUCLEO-F072RB, so the firmware has been written and tested only for these part numbers.

 

"If you feel a post has answered your question, please click ""Accept as Solution"""