Skip to main content
jvankuilenburg
Associate II
March 25, 2015
Question

HFI with STEVAL-IHM042V1

Posted on March 25, 2015 at 13:38

Hi,

I like to test the HFI function on the STEVAL-IHM042V1. Without HFI is the motor running well. But how can I implemented the HFI? I followed the instruction of UM1052 page 65. But I can not configure the DAC in the STMCWB. Because DAC1 is used for the OCP and DAC2-pin is input for the MC1currentA. What's the best way to do this?

Thanks,
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards