Skip to main content
This topic has been closed for replies.

5 replies

ST Employee
October 6, 2021

Hi, Thanks you for your feedback.

I have try to reproduce your problem but without success.

Could you give me more details please ?

Have you modified the qml file or the json file?

BRs

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
MK.1
MK.1Author
Associate III
October 7, 2021

Hi,

Win7, X-Nucleo IHM08 + Nucleo 446RE, LL driver.

Pilot 5.y.3 default. In torque control mode, it is not possible to enter a value greater than 500 s16A.

Pilot 5.y.2 default. In torque control mode, it is not possible to enter a value greater than 4000 s16A.

In the position control mode, it is not at all clear what is displayed in the window TargetTorque. The value does not match any of the registers.

Best regards.

ST Employee
October 12, 2021

Hi,

You can modify the GUI to fit to your needs. Just edit DefaultApp.qml (in GUI Folder) iwth the values you want.

For example, for torque range you can modify the from and to property of spinbox of id: rampTargetTorque :

SpinBox {

id: rampTargetTorque

property real rampTorqueRefRegVal: mcRegBank.getRegisterByName( "I_Q_REF" ).value

from: -32768

to: 32767

......................

Anyway this will be fix in next release of MotorPilot.

For the position control mode which qml and register.json files do you use?

BRs

If you agree with my answer, please accept it by clicking on 'Accept as solution'.
MK.1
MK.1Author
Associate III
October 13, 2021

Hi!

I didn't know that you can change the interface with the qml file. Therefore, I used the default interface. Thanks for the advice to switch the interface to position control.

MK.1
MK.1Author
Associate III
October 13, 2021

I use RegListSTMV2.json

I switched the interface to position control mode (PositionControlApp.qml)

Communication breaks after trying to enter a value.

0693W00000FCKSsQAP.jpg0693W00000FCKRVQA5.jpg