Skip to main content
UHerd.1
Visitor II
April 20, 2020
Question

Hello, I want to use a STM32G474CBU with two motors, but I have the problem that I can't select "shared resources for both motors" in "Control Stage - Analog input and Protection". I am using MCSDK_v5.4.3.

If I select a SM32F303CB I can select "shared resources for both motors" using ADC1/2 for both motors. I don't understand why it works for the STM32F303CB and not for the STM32G474CBU.

Because of space and simple layout I want to use a STM32 in a UFQFPN48 case for two motors and 3-shunt measurement and Encoders.

It would be nice if someone can give me answer to my problem.

Best Regards,

Ulf

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

Adding of the "SM32 Motor Control" topic.

Best regards.