Skip to main content
AndreaC1985
Associate II
Oct 4, 2018 3:31 PM UTC
Solved

Hello, I'm reading the application note PDF AN2388 for induction motor control algorithm. Is available somewhere the full code to download? Is it available any other detail on the implementation of IFOC on ST microcontroller?

..

This topic has been closed for replies.
Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:57 PM UTC

Dear @AndreaC1985​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

1 reply

Laurent Ca...
Laurent Ca...Best answer
Senior III
Jun 28, 2021 12:57 PM UTC

Dear @AndreaC1985​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards