Question
has anyone succeeded to run the EVSPIN32F0602S1 ?
I have generated a project using ST Motor Control Workbench. I have compiled the project and downloaded to microcontroller. I can debbug the program but when I start Monitor from Motor Control Workbench and click on "Connect" I receive the message : " Connection failed! No response, check the communication cable, the power on the board or the baudrate (set to 19200 bps)."
The baudrate is set to 19200 in Monitor and in Device Manager.