Skip to main content
LFu.1
Associate II
September 16, 2021
Question

GPIO pin doesn't have output

I configure 6 channel GPIO pins to generate PWM signals to control 3-phase bridge. There is one pin(PC13) sometimes stop to generate signal. Even we reset 3.3V power voltage, it won't recover. one time I inject 20k square wave to pin PC13 to verify other chip, but it cause the processor recovered. I use pin PA7 to sampling voltage(use as internal op-amp ), it always has 1V even turn off 3.3V power. I am guessing because of this voltage cause the processor can't reset completely? How to explain these?

​

Thanks,​

This topic has been closed for replies.

2 replies

TDK
September 16, 2021

Sounds like there may be hardware issues going on. Pulling NRST low will reset the processor under normal scenarios.

If pins have a voltage on them while VDD is 0V, something external must be driving them high.

PC13 is special as it runs off of the low-power domain and has limited source/sink capability.

"If you feel a post has answered your question, please click ""Accept as Solution""."
LFu.1
LFu.1Author
Associate II
September 16, 2021

Thanks for your answer. How can we explain the processor can't get Reset properly. I guess it is because of PA7 has 1V voltage. But I am not sure. The issue didn't come up frequently. It is very hard to verify.