Skip to main content
SF??r
Associate III
Sep 10, 2024 11:34 AM UTC
Question

Formular of Feed Forward Control Constants

Hi,

 

the MotorControlWorkbench is generating the Feedforward control constants:

M1_CONSTANT1_Q

M1_CONSTANT1_D

M1_CONSTANT2_QD

How are the calculated, are there any documentation or formula for it?

The Feedforward seems to be relevant for my project because I see current ripple aligned with my DC bus voltage ripple. But in practice there is no improvement, if I activate the FeedForward control. Also the bus voltage is measured with 1 ms and a filter with 6 values is applied. Are there any tips for my application if I have a bus voltage ripple period of 10 ms (3 Phase, 50 Hz)?

 

Thanks for Help

 

Sebastian 

    2 replies

    roar
    Associate II
    Jan 13, 2026 2:03 AM UTC

    Also interested in how these constants are calculated. Did you find any information on this?

     

    Regards

    Roar

    Agran.1
    Associate III
    Sep 15, 2026 11:42 AM UTC

    Did you find the formula?
     

    Regards

    AG