Skip to main content
Jancho
Associate
October 27, 2019
Question

FOC SDK 5.4 - encoder

  • October 27, 2019
  • 1 reply
  • 572 views

Hi i have configured the  quadrature encoder in Motor->Sensors and set the number of pulses

and select the quadrature encoder in Drive Management->Speed/Position Feedback Management

for to finish set the correct IO pins used for the quadrature encoder in Control Stage->Digital IO. as A15 and B3.

After this, compile and load, but the motor does nos espin , what i have done wrong ?

Thanks

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards