Skip to main content
paul2
Associate III
October 9, 2017
Question

FOC SDK 4.3 | Motor Profiler | low power BLDC

  • October 9, 2017
  • 6 replies
  • 1564 views
Posted on October 09, 2017 at 08:04

We are trying to setup a small BLDC motor with the Motor Profiler utility.

-X-NUCLEO-IHM07M1

-FOC SDK 4.3

-Custom motor: 2 pole pair BLDC 18VDC, 2W @ no load, 4000 rpm

With this setup the Motor Profiler is not able to successfully finish the profiling sequence.

During the profiling cycle the motor is turning slower each profiling attempt during the determination of the electrical model. The sequence stops with the message: profiling sequence takes to long.

Why is the Motor Profiler utility not able to finish the profiler sequence using the BLDC motor mentioned above? Are there special modifications necessary running ‘low’ power BLDC motors?

This topic has been closed for replies.

6 replies

Teddy Chobtrong
Associate II
October 9, 2017
Posted on October 09, 2017 at 15:46

I have also got this problem. After I have set lower max. speed and max. current, the Motor Profiler is able to successfully create a motor profile.

paul2
paul2Author
Associate III
October 9, 2017
Posted on October 09, 2017 at 17:27

Hi,

we already tuned the motor at 0.28 Apk. This value is given as a minimum by the Profiler utility:

0690X000006048NQAQ.jpg

Did you use a max current < 0.28 Apk? What are your motor specs?

Teddy Chobtrong
Associate II
October 9, 2017
Posted on October 09, 2017 at 17:37

I used a 48V 15A 10-Pole motor. My setting is Max Speed 500 RPM and Max Current 12 Apk.

paul2
paul2Author
Associate III
October 12, 2017
Posted on October 12, 2017 at 21:57

Selected a BLDC motor which is running at 0.33 Apk which is higher then the minimum of 0.28 Apk. Profiling successfully within 10 seconds. Problem solved.

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards