Question
FOC motor run but RPM does not increase after certain limit, how to increase output power?
hi st community,
I am using NUCLEO-G431RB control board and STEVAL-IPM20B power board, generate the code using st-workbench. the board is connected with 1kw PMSM motor of 3000rpm.
Motor run fine up to 1200 rpm but rpm not increase after that, at that point the motor output power showing 200 W on monitor dial.
st work bench monitor screen has power dial of maximum 200W, is that limit or what? the power board capacity 2000W.
how can I achieve the full RPM with increase in output power.
thanks,