Skip to main content
paul2
Associate III
Oct 12, 2017 7:54 PM UTC
Question

FOC duration fault

Posted on October 12, 2017 at 21:54

Hi,

Running the configuration below:

-NUCLEO-F302R8

-X-NUCLEO-IHM07M1

-FOC SDK 4.3

Succesfully tuned BLDC motor with the Motor Profiler. Also in Play Mode the motor runs very well.

Next step is running the BLDC motor using Motor Control Workbench based on the configuration above and the saved motor profile.

Shortly after hitting the 'Start Motor' button the motor stops with fault 'FOC duration'. Increasing the Execution rate doesn't help.

Why does the motor runs well with Motor Profiler - Play Mode, but not with the Motor Control Workbench? What could be the issue here?

Thanks.

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
Jun 15, 2021 7:01 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards