Skip to main content
Quentin Ch
Associate III
November 21, 2022
Question

FOC command is sometimes stuck

Hello,

I'm controlling a BLDC motor with MCSDK 6.0.0 and IHM08M1, with FOC with 1024 PPR encoder. I compute torque (Iq_ref) commands to achieve speed control, this works ok except in rare case described below:

Sometimes the MCSDK seems "stalled":

  • I send a torque (Iq_ref) command, but the motors does not run
  • The motor can mechanical spin freely (not blocked, I can spin it manually). Even I I release completely the load, is does not spin.
  • Encoder feedback is ok (the MCSDK return a speed if I turn the motor manually)
  • The PI current loop and the PWM regulation seem running since the read Iq value oscillates around the Iq_ref I set. Some current is flowing since the MOSFET are a little (be reasonably) hot.
  • No fault flag is set
  • Resetting the controllers solves the issue.

Why such behaviour could appear ?

Any clue ?

NB: this seems to occurs when I set a torque command to move the motor starting from 0 rpm.

Thanks,

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
November 24, 2022

Hello,

Did you check that, after your torque (Iq_ref) command, the internal I_Q_REF register is set accordingly? You can display it with the motor pilot register tab...

What is the control board type?

Best regards.

GMA

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA