Skip to main content
Cpiac.1
Associate
September 15, 2021
Question

flash memory in stspin32f0 is full just creating the source code with MotorControl Workbench 5.Y.2, is this normal ?

Dear all, if the answer at my above question is:"YES" and the available space is already full...does is there a compatible chip with larger memory? or did I make some mistake? any suggestions?

See below pict for better understanding

Cristiano

This topic has been closed for replies.

5 replies

Cristiana SCARAMEL
ST Employee
September 15, 2021

Hello @Cpiac.1​ and welcome to the ST Community.

The picture is missing ;)

However, which IDE are you using?

"If you feel a post has answered your question, please click ""Accept as Solution"""
Cpiac.1
Cpiac.1Author
Associate
September 17, 2021

I'm using STM32CubeIDE 1.6.1.

best regards.

Cristiana SCARAMEL
ST Employee
September 17, 2021

Hi @Cpiac.1​ ,

please could you attach the picture above mentioned.

"If you feel a post has answered your question, please click ""Accept as Solution"""
Cpiac.1
Cpiac.1Author
Associate
September 20, 2021

0693W00000DnhxfQAB.jpgBye.

Cristiana SCARAMEL
ST Employee
September 22, 2021

Hi @Cpiac.1​,

are you using the HAL APIs? 

A first step of optimization could be use the Low Layer APIs in the ST Motor Control Workbench.

In addition you can use the compiler optimization in the STM32CubeIDE.

Since your question is about STM32 MCSDK, I added the topic "STM32 Motor Control" user of this community are experts of ST Workbench and can help you.

Anyway, I can suggest as an alternative the last SIP STSPIN32G4 that embeds STM32G431 MCU (128 kB Flash memory).

"If you feel a post has answered your question, please click ""Accept as Solution"""