Skip to main content
Thierry BABONNEAU
Visitor II
April 3, 2018
Question

Flag and status feedback description in the FOC 4.3 serial communication

Posted on April 03, 2018 at 11:38

I would like to use the serial protocol to communicate with the FOC 4.3. I need to have a feedback of the motor status (overcurrent fault..). Two readable registers (status ans flags) are described in the user manual (UM1052 p164) but I can't find any precise description of each bit of this registers.

Thanks by advance for your help.
This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards