Skip to main content
FMaur.1
Visitor II
August 18, 2021
Question

Field oriented control with STEVAL-SPIN3201: Why does Motor always stops right after start up with speed feedback or start-up failure?

Hello,

I have big troubles driving a motor with the STEVAL-SPIN3201 using FOC-Algorithms.

The motor is connected to the board and the code is generated using the MC workbench.

The motor always starts turning but then suddenly stops. I think it is the moment, when the final value of the speed ramp is reached. The motor pilot then shows speed feedback or start-up failure. I already tried different parameter settings.

Do you have an idea about the cause of this problem?

It would be great if you could help me.

Best regards,

Florian

This topic has been closed for replies.

2 replies

Enrico Poli
ST Employee
August 20, 2021

Added STM32 Motor control topic

ARaj.1
Associate II
August 21, 2021

Your PWM frequency maybe too high. Anything above 15-16kHz caused problems as the PWM frequency is also what's used to trigger FOC calculation, and if the calculation takes longer than the period of the frequency you will get FOC error.