Skip to main content
Associate II
Oct 31, 2025 4:22 AM UTC
Question

EVSPIN32G4 – Motor 2 not rotating in Sensorless FOC (works in MC Workbench 6.3.2 but not in 6.4.1)

 

I’m using the EVSPIN32G4 dual motor control board with MotorControl Workbench 6.4.1 in Sensorless FOC mode.

Both motors have identical configurations, but Motor 2 doesn’t rotate when using Workbench 6.4.1.
The same setup works perfectly in Workbench 6.3.2, where both motors run normally.

Hardware and wiring are fine — this seems to be a software or code-generation issue in Workbench 6.4.1 for dual-motor projects.

Can you please confirm if this is a known issue or regression in version 6.4.1, and suggest a fix or workaround?



Setup Summary:

  • Board: EVSPIN32G4

  • Mode: Sensorless FOC, Dual Motor

  • MC Workbench: 6.4.1 (issue), 6.3.2 (working)

  • IDE: STM32CubeIDE 1.19.0

6 replies

GMA
ST Technical Moderator
Oct 31, 2025 8:22 AM UTC

Hello @Chandana_Arava,

Is an error reported?
From my side, both motors operate with the same configuration in STO-PLL.
Can you share your .stwb6 file?

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate II
Nov 4, 2025 5:26 AM UTC

Sorry for the late reply,
No error got reported from my side, I am sharing .stwb6 file .
Please check and let me know what might be cause for it and how to resolve that.

GMA
ST Technical Moderator
Nov 4, 2025 9:56 AM UTC

Hello @Chandana_Arava,

The M2 driving topology has been modified for your use case. As mentioned in the workbench tool, hardware modifications must be implemented.

GMA_0-1762249691560.png

Using your STWB6, with the default driving topology (U, V, W, shared enable) and without hardware board modification, the M2 motor spins.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Associate II
Nov 4, 2025 10:16 AM UTC

Hello @GMA ,

In this case, I am using the M1 modified driving topology, as shown in the attached file. Should I modify that file as well, or is it already suitable for M1?

Associate II
Nov 10, 2025 3:49 AM UTC

Can you please conform the solution so that I can move forward.

Thanks & Regards,
Chandana Arava.

GMA
ST Technical Moderator
Nov 12, 2025 8:20 AM UTC

Hello @Chandana_Arava,

Your last picture displays the M2 settings, not the M1 settings.
In your Ready_to_sky_920KV_Dual_V2.stwb6 file, you are using the default configuration for M1, while the M2 configuration has been modified. For M2, hardware modifications must be performed as mentioned in:

GMA_2-1762935605622.png

 

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA