EVSPIN32G4-DUAL Second Motor will not spin
- 2 replies
- 1421 views
Hello,
I am trying to evaluate the use of MCSDK in a dual-motor application. Motor 1 works, but motor 2 does not.
I have a fresh Workbench project, with both motors configured identically, with the exception of Over-Current Protection. When I generate, I get a "NOTICE: Please disable the overcurrent protection of Stage 2 to avoid resource assignment conflict on COMP2. The power state is already protected by STDRIVE101." Under Current Sensing of Stage 2, I disabled Over-Current Protection, but still get the notice.
The generated CubeIDE project compiles and uploads without issue.
I use MC_FOC_SDK_2_Motors to try to start/stop the motors. After connecting, I hit press Start on Motor 1. I hear the PWM, and after a second (as expected), the motor starts ramping according to my startup sequence. When I press Start on Motor2, I get no sound, and no motion.
I analyze the outputs to the motor with a dual channel oscilloscope. On Motor 1, U, V, W signals are in phase, with varying pulse width. On Motor2, U, V, W signals are identical in pulse width and phase, which is consistent with no motion and no sound, but I have no idea why it does that.