Skip to main content
ST Migration account
ST Community Manager
Aug 22, 2026 5:01 PM UTC
Solved

EVSPIN32G4 current sensing with 3-shunt

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.


Hello.

I am creating a motor control project for the EVSPIN32G4 using MotorControl Workbench 6.4.1.
The EVSPIN32G4 board definition provides configurations for "ThreeShunt_RawCurrents_SingleEnded_ExternalGain" and "ThreeShunt_RawCurrents_SingleEnded_InternalGain," but the current sensing section in the circuit diagram of this board appears to match the "ThreeShunt_RawCurrents_Differential_ExternalGain" configuration.

However, adding this configuration causes MotorControl Workbench to fail with an error. This is likely because the definition for "ThreeShunt_RawCurrents_Differential_ExternalGain" does not exist for the STSPIN32G4 in "MC_SDK_6.4.1UtilitiesPC_SoftwareSTMCWBassetsConnectionParameters.json".

1. Why is it that the EVSPIN32G4 schematic shows a differential configuration, but the board definition only provides a single-ended option?

2. Is it possible to edit "ConnectionParameters.json" and add the "ThreeShunt_RawCurrents_Differential_ExternalGain" definition to use this configuration in MotorControl Workbench?

Thanks in advance and best regards.

GMA
GMABest answer
ST Technical Moderator
Aug 22, 2026 5:09 PM UTC

Hello ,

For the ThreeShunt_RawCurrents_Differential_ExternalGain_FilteredADCInput configuration, the statement is correct. For more details, refer to the board description wiki page available here. 
ThreeShunt_RawCurrents_SingleEnded_(InternalGain/ExternalGain) is the default three-shunt configuration used on the EVSPIN32G4 board.

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA

3 replies

GMA
ST Technical Moderator
Aug 22, 2026 5:04 PM UTC

Hello ,

The best solution for your use case could be to use the ThreeShunt_RawCurrents_Differential_ExternalGain_FilteredADCInput hardware variant. 
Each ADC input is low-pass filtered and this allows to use the HSO sensor less algorithm (refer to "HSO Startup Guide" available through "Workbench tool">About>Documentations>Documentation).

Non-HSO sensor less algorithm does not support the ThreeShunt_RawCurrents_Differential_ExternalGain hardware variant.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
ST Migration account
ST Community Manager
Aug 22, 2026 5:07 PM UTC

To adopt the ThreeShunt_RawCurrents_Differential_ExternalGain_FilteredADCInput configuration, the following 4 pins are required per phase:
?CURRENT_SHUNT_*P
?CURRENT_SHUNT_*N
?CURRENT_AMPL_*
?CURRENT_FILT_*
However, since there are few available pins and the filter circuit is not implemented on the EVSPIN32G4 board, and adding a new circuit is difficult, we believe this configuration is not feasible.


To be honest, I believe any configuration is acceptable as long as there are no problems with motor control on the EVSPIN32G4 board.
Currently, the most promising configuration is the ThreeShunt_RawCurrents_SingleEnded_ExternalGain configuration, which is defined by default in EVSPIN32G4.json. Would it be alright to adopt this configuration?

This account only shares restored community content posted by members between May 22 and June 9, 2026, who did not register for the new community.
GMA
GMABest answer
ST Technical Moderator
Aug 22, 2026 5:09 PM UTC

Hello ,

For the ThreeShunt_RawCurrents_Differential_ExternalGain_FilteredADCInput configuration, the statement is correct. For more details, refer to the board description wiki page available here. 
ThreeShunt_RawCurrents_SingleEnded_(InternalGain/ExternalGain) is the default three-shunt configuration used on the EVSPIN32G4 board.

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA