Skip to main content
Associate II
Mar 6, 2026 3:25 PM UTC
Solved

EVSPIN32G4: Current sense feedback resistor values

I all,
I have a question regarding the EVSPIN32G4 board, specifically concerning the feedback resistors used in the current sensing network (default value: 11 kΩ).

I am considering replacing them with 150 kΩ resistors. My main concern is whether this significant change will trigger the Overcurrent Protection (OCP) prematurely or cause stability issues with the internal op-amps.

Has anyone experimented with such values, or are there specific hardware limitations I should be aware of?

Best regards, Jules

AScha.3
AScha.3Best answer
Super User
Mar 9, 2026 11:43 AM UTC

Seems you could try this, with 150k + 2x 300k , to get a 2A max. range (about) . But you get high impedance then, very sensitive to stray in.

Bildschirmfoto_2026-03-09_12-34-24.png

But why not reducing the input of the diff-amp , R44 + 50 ?  try 1k5 -> 150 r , so you get 10x gain and 1/10 current range; you really need only so low range ?

 

 

If you feel a post has answered your question, please click on " Best Answer ".

3 replies

AScha.3
Super User
Mar 7, 2026 8:09 AM UTC

Hi,

just : WHY you want replacing them with 150 kΩ ? ( = this spoils the opamp bridge. )

+

Now -with 11k - the current measuring range of the opamp -> ADC is about 0...50A ;

this matches the capability of the board (and the 100A mosfets) quite good;

your change would spoil the opamp bridge and give a range of about 0...3 A , what seems quite useless to me.

If you feel a post has answered your question, please click on " Best Answer ".
JulesCAuthor
Associate II
Mar 9, 2026 11:13 AM UTC

Hi @AScha.3,

Thanks for the response.

I thought I could get better precision because I don't need such a wide range, as I am operating with small motors. But, based on what you’re saying, it seems I would be sacrificing stability or hitting the op-amp's limits ? Even if I change the resistors R41 & R47 to 300kOhm ?

 

 

AScha.3
AScha.3Best answer
Super User
Mar 9, 2026 11:43 AM UTC

Seems you could try this, with 150k + 2x 300k , to get a 2A max. range (about) . But you get high impedance then, very sensitive to stray in.

Bildschirmfoto_2026-03-09_12-34-24.png

But why not reducing the input of the diff-amp , R44 + 50 ?  try 1k5 -> 150 r , so you get 10x gain and 1/10 current range; you really need only so low range ?

 

 

If you feel a post has answered your question, please click on " Best Answer ".