Skip to main content
ketchup
Associate III
February 28, 2022
Question

EVSPIN32G4 CLONE - MC_BREAK_IN Error (MC 5.Y.3)

I designed clone of EVSPIN32G4 and can't resolve issue.

I generated application for EVSPIN32G4 and motor rotate without any problem, but on my PCB I have MC_BREAK_IN. Why TIMx_BRK_M1_IRQHandler() function is called?

I can't find issue in my design - it should be 100% compatible with EVSPIN32G4.

Could someone give me a hint for this issue. I can send example project for EVSPIN32G4 and my PCB design.

Best regards

�?ukasz �?ęcki

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
August 30, 2023

Dear ketchup,

Firstly, we would like to sincerely apologize for the delay in replying to your post.
If your point is still pertinent, BRK interrupt occurs if an over current is detected. The break in signal comes from internal comparators. Please refer to UM2850   "Embedded comparators" chapter for more detail. 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA