Skip to main content
Visitor II
Jul 21, 2025 7:00 PM UTC
Question

EVSPIN32G06Q1S3 and STLINK-V3SET not communicating

I am working with the EVSPIN32G06Q1S3 and the STLINK-V3SET, I have the two programmer/debugger boards mounted on top of each other. Then I have the UART connector connected to the EVSPIN32G06Q1S3 (J5) and the programmer/debugger boards (CN7). I have 230 VAC going into the EVSPIN board. The lights on both the STLINK and the EVSPIN turned on. Device manager recognizes the LINK, but I can't detect the EVSPIN in Motor Pilot or STM32CubeIDE. I've tried the "Discover Board" option in Motor pilot and manually changing the baud rate to each option with no results. I think it might be a firmware issue, but I'm not entirely sure. 

This topic has been closed for replies.

2 replies

GMA
ST Technical Moderator
Jul 23, 2025 4:07 PM UTC

Hello @Hugo_,

With STM32CubeIDE tool, you can try to upgrade the ST-LINK version:

GMA_1-1753286794402.png

 

 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
Billy OWEN
ST Employee
Aug 11, 2025 10:40 PM UTC

Hi @Hugo_ 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy