Skip to main content
Karan 123
Senior
June 14, 2021
Solved

EVSPIN32F601S3 + MOTOR PROFILER

Hi,

Is there any way to use Motor Profiler with EVSPIN32F601S3 Board ?

--

Karan

This topic has been closed for replies.
cedric H
cedric HBest answer
ST Technical Moderator
June 15, 2021

Hello Karan,

The EVSPIN32F0601S3 board is based on the STSPIN32F0601 controller which embeds a Cortex M0.

As Cortex M0 does not have FPU, Motor profiler can not be developed for this board.

Regards

Cedric

5 replies

cedric H
cedric HBest answer
ST Technical Moderator
June 15, 2021

Hello Karan,

The EVSPIN32F0601S3 board is based on the STSPIN32F0601 controller which embeds a Cortex M0.

As Cortex M0 does not have FPU, Motor profiler can not be developed for this board.

Regards

Cedric

Karan 123
Karan 123Author
Senior
June 15, 2021

Thanks.. for update..OK ..

Any other board compatible with NUCLEO-F302R8 for High Voltage BLDC Development . supports Motor Profiler ?

Input voltage from 50 V to 280 V DC/AC

--

Karan

cedric H
ST Technical Moderator
June 15, 2021

All available combinations control + power boards are showed in Motor profiler tool. Click on "select boards" button from the main window to have access to all of them.

Cedric

Karan 123
Karan 123Author
Senior
June 15, 2021

Ok.. Thanks ..

No Combinations for Input voltage from 50 V to 280 V DC/AC ?

--

Karan

Associate
July 18, 2023

Were you able get a solution on this?