Skip to main content
Associate
Jun 19, 2026 3:19 PM UTC
Question

EVSPIN32F06Q1S1 cant write code. i couldnt see the pin mapped like stm32

We are using the EVSPIN32F06Q1S1 board and have configured TIM1 PWM outputs as CH1/CH1N → PA8/PA7, CH2/CH2N → PA9/PB0, and CH3/CH3N → PA10/PB1. While probing the board, we observed PWM waveforms at test points TP1, TP2, and TP3, which according to the documentation are connected to RES1, RES2, and RES3 rather than to PA8, PA9, and PA10. The complementary outputs are also present and behaving as expected at their respective MCU pins. Could you please clarify how the TIM1 PWM signals are being routed to TP1–TP3 and whether RES1–RES3 are internally connected to the TIM1 outputs on this board?

1 reply

GMA
ST Technical Moderator
Jul 10, 2026 8:45 AM UTC

Hello ​@sagars,

Refer to the STSPIN32F0601 datasheet documentation available here for the High and Low side signals management.
 

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA