Skip to main content
Associate
Jun 22, 2026 5:27 AM UTC
Question

EVSPIN32F0602S1 how do i configure this board with ide

I am new to this evaluation boad can someone please help me to configure this board. is there any separate ide for this other than cube ide?

3 replies

GMA
ST Technical Moderator
Jul 10, 2026 7:46 AM UTC

Hello ​@sagars,

The EVSPIN32F0602S1 board is available in the Motor Control software development kit (SDK).
Refer to the Getting started with Motor Control SDK chapter of the user manual available in MC Workbench > About > Documentations > Documentation.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA
sagarsAuthor
Associate
Aug 11, 2026 4:14 AM UTC

I am planning to use this board to run turbo molecular pump with 56VAC and up to 800Hz of frequency. how can i customize the motor or how can i put this motor into the mc workbench. all I need to generate 56 VAC at 800 Hz at the output.

GMA
ST Technical Moderator
Aug 11, 2026 3:54 PM UTC

Hello ​@sagars,

The JSON motor description file can be created with the MC Profiler by using a board that supports this feature. Refer to the Motor Profiler Application Note in the user manual for MC Workbench documentation.

Alternatively, some motor parameters can be computed by using the How To manually configure the motor parameters wiki page. Set inertia and friction parameters to nonzero values. The PID speed parameters will need to be tuned in this case.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA