Skip to main content
SLodo.1
Associate
Aug 26, 2020 7:18 AM UTC
Solved

EVSPIN32F0601S3 + ST Motor Profiler

Hey. When will it be possible to add the EVSPIN32F0601S3 board to the ST Motor Profiler? Or which one to choose from the proposed for determining the parameters of the electric motor?

This topic has been closed for replies.
Enrico Poli
Enrico PoliBest answer
ST Employee
Aug 27, 2020 2:13 PM UTC

Hi @SLodo.1​ , unfortunately the EVSPIN32F0601S3  is not supported by the motor profiler.

However you can collect the motor characteristics using the STEVAL-IPM05F as power board.

4 replies

Enrico Poli
Enrico PoliBest answer
ST Employee
Aug 27, 2020 2:13 PM UTC

Hi @SLodo.1​ , unfortunately the EVSPIN32F0601S3  is not supported by the motor profiler.

However you can collect the motor characteristics using the STEVAL-IPM05F as power board.

Karan 123
Senior
May 10, 2021 4:30 PM UTC

Hi @Enrico Poli (ST Employee) , SLodo.1 (Community Member)

Which combination should I use for EVSPIN32F0601S3 in Motor Profiler 5.4.6?

0693W00000ANtnEQAT.png 

How the hardware ( Nucleo Board + STEVAL-IPM05F) will be identical/matched with EVSPIN32F0601S3 to Run Motor Profiler ?

or you suggest buy another board?

Thanks in advance ..

--

Karan

SLodo.1
SLodo.1Author
Associate
Jun 28, 2021 5:18 AM UTC

Any pair of equipment can be used (also in conjunction with nucleo 103). The choice of power section depends on the capacity and power supply of your drive. Then you can use EVSPIN32F0601S3 to mcwb to create a project with parameters from Motor Profiler.

Laurent Ca...
Senior III
Jun 28, 2021 4:33 AM UTC

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards