Skip to main content
jorge2
Associate II
April 20, 2016
Question

Evaluating Motor Control using AC6 Workbench for STM32

Posted on April 20, 2016 at 19:52

Hello, I am trying to evaluate motor control firmware with AC6 Workbench. I am looking at the STM32 PMSM FOC SDK 4.2, Hands-on workshop with hardware tools, Rev 1.5, and it only supports Keil and IAR. Is there a version for AC6 Workbench?

Thanks.

This topic has been closed for replies.

2 replies

Gigi
ST Employee
April 21, 2016
Posted on April 21, 2016 at 08:31

Ciao

No I'm sorry. At the moment the workspaces for AC6 is not provided with the last release of the MC FOC Lib.

Ciao

Gigi

Laurent Ca...
Senior III
June 17, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards