EVALSTDRIVE601 Failure and IGBT Destruction at 600V
- 6 replies
- 621 views
Hello,
I am using the EVALSTDRIVE601 evaluation board (featuring the STDRIVE601) to try to generate a controllable three-phase signal. I wired the evaluation board exactly as described in the datasheet:
HV and PGND (J1 connectors): Connected to the DC voltage source.
SGND and VCC (J3 connectors): Connected to the ground and output of a buck converter that steps down 24V to 12V.
VDD: Connected to the 3.3V of the MCU.
Pin 1 (Fault): Connected to the MCU to read this value and detect fault conditions.
Pins 3, 5, 7, 9, 11, and 13: Connected to the SPWM signals. I am generating these using a Compute Module 4 with a switching frequency of 10kHz and a modulating frequency of 50Hz.
Pin 23 (Enable): Connected to the MCU, providing 3.3V to activate the driver.
Pin 2: Connected to the GND of the MCU.
Pin 28: Connected to the 3.3V of the MCU.
Test 1: 24V DC with LC Filters I initially tested the board using an external 24V DC power supply. At the output (J2 connectors), I wired an LC filter (L = 680mH, C = 47µF) on each of the three phases. This test worked perfectly, and I was able to generate a controllable three-phase AC signal.
Test 2: 600V DC without Load Next, I tested the board at 600V DC. I started with nothing connected to the J2 output connectors. When I activated the Enable pin with a duty cycle of 10%, a signal resembling a sine wave was generated, which I measured using a voltage probe connected to an oscilloscope between phase 1 and 2 of the J2 connectors. However, this signal was not stable. After a couple of seconds, the signal was completely attenuated, and a fault appeared on Pin 1. This correctly disabled the Enable pin and turned off the SPWM signals (which are inverted, as specified in the datasheet).
Test 3: 600V DC with LC Filters and Board Failure I then tried testing at 600V DC with the LC filters connected to the three phases. This time, when I activated the Enable pin with a 10% duty cycle, I immediately read a fault on Pin 1 and no signal was generated.
I retested while observing the VCC pin of the J3 connectors to check if an undervoltage condition (VCC UVLO) was being detected, but the VCC remained perfectly stable at 12V. While investigating this error condition—and importantly, while the Enable pin was inactive—the 6 IGBTs integrated into the evaluation board brutally exploded, destroying the board as seen in the attached picture.
If possible, could I get some assistance regarding this issue? I am available for any clarifications. If you notice any mistakes I made with my connections or my testing procedure, please let me know.
Thank you in advance for your time and help.