Skip to main content
NK.13
Associate II
Jul 24, 2019 9:56 AM UTC
Question

Error in code which is generated by St motor workbench

i have generated code from motor control workbench and when i build this code the error came as,

region `FLASH' overflowed by 18000 bytes StSpin_Hall_24_07 C/C++ Problem

StSpin_Hall_24_07.elf section `.text' will not fit in region `FLASH' StSpin_Hall_24_07 C/C++ Problem

i tried for optimised the code code then the there is no error but motor is not working well.......

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
Jun 22, 2021 8:21 AM UTC

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards