Skip to main content
slagment
Associate II
April 16, 2012
Question

Encoder, Direction Bit toggles with every Pulse, Count 1 or 0.

Posted on April 16, 2012 at 23:13

Hello, I've set up a STM32 with an incremental optical two channel encoder.

The counter direction bit toggles between 0 and 1 every count. As a result, the counter never gets pass 1. The counter reads 0,1,0,1,0,1... I've tried all the counter modes, polarity settings, and channel counting settings. Has anyone experienced this before? Any ideas? Thanks

void ecdr_TIM2_init(void)
{
//Enable bus.
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE); 
//Setting encoder inputs.
GPIO_init(GPIO_Mode_AF, GPIO_OType_PP, GPIO_Speed_25MHz, GPIO_PuPd_NOPULL, Encoder_TIM2);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource1 | GPIO_PinSource0, GPIO_AF_TIM2);
// NVIC_InitTypeDef NVIC_InitStructure; //Hold intr settings.
//Enabling interrupts for Timer 5.
// NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn;
// NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
// NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
// NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
// NVIC_Init(&NVIC_InitStructure); //Set control reg.
TIM_TimeBaseInitTypeDef TIM_base;
TIM_base.TIM_Prescaler = 1; //Prescale.
// TIM_base.TIM_CounterMode = TIM_CounterMode_Up; //Up-counter. Should be adjusted be Enc interface.
TIM_base.TIM_Period = 0xFFFF; //Auto-reload register.
// TIM_base.TIM_ClockDivision = 0; //Filter sampling.
// //Enable timer.
TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising,TIM_ICPolarity_Rising); //Enable encoder interface. 
TIM_TimeBaseInit(TIM2, &TIM_base); //Set register settings.
//TIM_PrescalerConfig(TIM2, 1, TIM_PSCReloadMode_Immediate); 
TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI12, TIM_ICPolarity_Rising,TIM_ICPolarity_Rising); //Enable encoder interface. 
TIM_Cmd(TIM2, ENABLE); 
// TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); 
} 

#stm32-encoder-direction
This topic has been closed for replies.

1 reply

slagment
slagmentAuthor
Associate II
April 18, 2012
Posted on April 18, 2012 at 18:43

Problem found.

Can't | GPIO_PinSource.

GPIO_PinAFConfig(GPIOA, GPIO_PinSource1 |  GPIO_PinSource0, GPIO_AF_TIM2);

Change to:

GPIO_PinAFConfig(GPIOA,GPIO_PinSource0, GPIO_AF_TIM2);

GPIO_PinAFConfig(GPIOA, GPIO_PinSource1, GPIO_AF_TIM2);