Skip to main content
Visitor II
Jul 31, 2025 1:23 PM UTC
Question

Electrical Angle Synchronization in MCSDK v6.4.0 to avoid long-term drift.

Question about Electrical Angle Synchronization in MCSDK v6.4.0

Hi everyone,

I'm using MCSDK v6.4.0 with an STM32G4, a 42BLF01 motor, and a high-quality incremental encoder with Z-index.

My goal is to accurately correct the electrical angle on each Z-pulse to avoid long-term drift after 100 rounds.

In previous SDK versions, there was a function called ENC_SetElAngle() which allowed setting the electrical angle directly.
In MCSDK v6.4.0, however, this function no longer exists – and the corresponding enc_driver.h file is also missing.

Main Question:

Is there any official or recommended way in MCSDK v6.4.0 to directly set or correct the electrical angle at the Z-pulse – without using ENC_SetElAngle()?

If not:

  • What’s the recommended strategy for drift-free synchronization while the motor is running?

  • Is MC_SetCtrlPositionAngle1() the intended method – even though it may cause stepping or jitter?

Thanks for any insights

This topic has been closed for replies.

1 reply

GMA
ST Technical Moderator
Aug 4, 2025 8:31 AM UTC

Hello @Baumi,

Which version are you referring to for "previous SDK versions"?
The ENC_SetMecAngle() function is available in the encoder_speed_pos_fdbk.c file located in the Project\MCSDK_v6.4.0-Full\MotorControl\MCSDK\MCLib\Any\Src directory.

If you agree with the answer, please accept it by clicking on 'Best answer'.Best regards.GMA