Skip to main content
cyt
Associate II
January 8, 2020
Question

electrical angle question

As described in 

UM1052 User manual STM32F PMSM single/dual FOC SDK v4.3

8.3.3 Setting up the system when using Hall-effect sensors

For these reasons, it is suggested to follow the instructions given below when connecting a

Hall-sensor equipped PM motor to your board:

2. Turn the rotor by hand in the direction assumed to be positive and look at the B-emf

induced on the three motor phases. If the real neutral point is not available, it can be

reconstructed by means of three resistors, for instance. 

...

6. Enter two parameters displacement and delay found in the ST MC Workbench GUI,

inside the window related to motor speed and position sensor. An example with delay

equal to 270° is illustrated in Figure 85: "Determination of Hall electrical phase shift"

My question:

If I Turn the rotor by hand in the direction assumed to be "negative", 

how to calcuate the delay? same as "positive"? any difference if I trun the rotor by hand in "negative" direction?

Thanks

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards