Skip to main content
5628512363462302E12
Visitor II
July 24, 2019
Question

Drive a sensored-BLDC motor

  • July 24, 2019
  • 1 reply
  • 908 views

Hello everyone!

I tried to drive a BLDC motor with hall sensors. I used the SPIN3202 board.​ But I always get "Speed feedback" error and the motor cannot even start.

I checked the "STM32 PMSM FOC SDK Frequently-asked questions (FAQ)" and for "Speed feedback" the answer is using speed ramps. But if I selected hall-sensor "speed sensing", there is no "start-up parameters" under "Drive management" anymore.

0690X000009Z3PkQAK.png

Does anybody has the same problem and how did you solve it? Or how do you drive a sensored-BLDC with ST control board?

Thanks!

This topic has been closed for replies.

1 reply

Laurent Ca...
Senior III
June 15, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards