Skip to main content
LXian.0
Associate II
July 3, 2019
Question

Drive 48V Conveyor Drum Motor using STEVAL-SPIN3201

Hello Community,

I have purchased a STEVAL-SPIN3201 eval board last week. I want to drive a 48V Drum motor using this eval board with Motor Control Workbench 5.40. But I don't have the full motor parameters. Based on the user manual UM2152, the motor parameter configuration need to modify if different motor application is used and then generate new firmware code download into the eval board. My question is anyone tried this kind of motor using Motor Control Workbench 5.40. If yes, can you share how's the configuration

The motor information below is all I have:

Rated voltage: 48V

Rated current: 6A

number of Poles: 10

0690X000009YKdRQAW.jpg

Thanks.

Regards,

XH Low

This topic has been closed for replies.

3 replies

cedric H
ST Technical Moderator
July 9, 2019

Hello,

Every motor are different, and I would advise you to characterize it manually.

I attach to this post the procedure we used in order to do so.

Regards

Cedric

LXian.0
LXian.0Author
Associate II
July 10, 2019

Thanks Cedric.

Let's see I can measure the motor parameters.

Regards,

XH Low

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards