Question
Does STM32G431V8 controller has Motor control and Interleaved PFC compatibility and software package available which can be used to run and control the motor with minimum software efforts?
We are planning to use this controller for our new VFD design. I need to know in detail about this controller:
- We know this controller can be used for controlling one Motor and one PFC. Is there the motor control and PFC software package readily available for these controllers? If so, with minimum software efforts, can we able to run the motor? Or do we need to put more efforts to develop the software?
- Is it possible to use this controller for 2 phase interleaved PFC control as well?
- If it can be configured for the interleaved PFC, then the software required for interleaved PFC control is readily available with TI or we need to develop?
- Is it possible to control the 2nd low power motor (for 250W Fan control motor, 3 ph inverter) along with Main motor control with this single controller?
- If not, is there any other controller available to control two motor and two phase interleaved PFC control?