Skip to main content
Ysiu
Associate
July 26, 2019
Question

Does STM32F303RE support dual motor drive?

Hi there, I am using ststem workbench for stm32, cube mx v 5.3 and mcsdk 5.4. I want to develop a dual motor application with stm32f303re. However, after I generate the code and upload it. It cannot connect through the monitor. (Works for single motor). What would be the potential problem? I would be very appreciate and gratful for receiving any of your suggestions.

This topic has been closed for replies.

2 replies

Ysiu
YsiuAuthor
Associate
July 26, 2019

HI for anyone encounter the same problem. I just solved this issue. Before assigning pin in st motor control workbench, please check if the pin really exsist on the chip. If you assign a pin which is doesn't exist, error occurs.

Laurent Ca...
Senior III
June 22, 2021

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards